How can we help you today?

M251/M241 What happens to the program (boot application) if there is a power outage and there is no battery (or it expired and it was not replaced)

->Issue:

What happens to the program (boot application) if there is a power outage and there is no battery (or it has expired and it was not replaced)

->Product Line:

Machine Expert

->Resolution:

The battery only works to keep the internal clock running while there's no power in the PLC. It has nothing to do with the project being loaded into the controller.

The boot program is stored in the flash memory, which does not require battery backup; in case of a power outage you won't lose the program.

You can clone the application on an SD Card and have it as a backup just in case you need to put it into a replacement PLC if the PLC happens to be damaged in the future.

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.If you are not located in North America, please contact your local Customer Care Center for assistance:Support | Schneider Electric Global (se.com)

Schneider Electric Nigeria