Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Where to Find the DTM Version Matrix for Control Expert v16.2 and Older Versions ?

Please refer to the DTM Version Matrix below, which corresponds to CE v16.2 and previous versions.

Control Expert Version
DTM Name14.014.0 Hotfix14.114.1 Hotfix15.015.0 SP115.115.215.316.016.2
BME NOC 03x1.x2.12.202.12.232.13.362.13.372.14.232.14.482.15.722.16.292.17.242.19.693.0.10.0
BME H58 x0402.12.202.12.232.13.362.13.372.14.232.14.482.15.722.16.292.17.242.19.693.0.10.0
BME P58 x0x02.12.202.12.232.13.362.13.372.14.232.14.482.15.722.16.292.17.242.19.693.0.10.0
BME H58 x040S2.12.202.12.232.13.362.13.372.14.232.14.482.15.722.16.292.17.242.19.693.0.10.0
BME P58 x040S2.12.202.12.232.13.362.13.372.14.232.14.482.15.722.16.292.17.242.19.693.0.10.0
NOC 78x002.12.72.12.72.13.322.13.322.14.112.14.262.15.242.16.122.17.112.19.132.21.40.0
NOC 78x00.22.12.72.12.72.13.322.13.322.14.112.14.262.15.242.16.122.17.112.19.132.21.40.0
M_NOC 04023.12.73.12.73.13.343.13.343.14.113.14.283.15.263.16.123.17.113.19.153.21.39.0
Advanced_Generic_EDS1.8.51.8.51.9.321.9.321.10.111.10.241.11.231.12.121.13.111.15.131.17.39.0
Generic_Device1.8.51.8.51.9.321.9.321.10.111.10.241.11.231.12.121.13.111.15.131.17.39.0
Modbus_Device1.2.51.2.51.2.51.2.51.2.51.2.141.3.21.4.01.5.01.7.21.9.39.0
BME CXM 01001.00.00031.00.00031.00.00031.00.00031.00.00031.00.00041.00.00071.00.00081.00.00081.00.00081.00.009
PME Generic DTM1.0.321.0.321.0.321.0.321.0.321.0.321.0.371.0.371.0.371.0.41(*)1.0.45
BME AHI 08121.1.71.1.231.1.71.1.71.1.91.1.121.1.201.1.201.1.201.1.221.1.23.0
BME AHO 04121.1.71.1.231.1.71.1.71.1.91.1.121.1.201.1.201.1.201.1.221.1.23.0
BME NOR 2200NANANA1.0.0611.0.0872.1.20353.13.0.22049.13.0.22055.13.0.22308.14.0.23311.24.1.24326.1
ModbusPlaceHolderNANANANA1.0.91.0.181.0.221.0.221.0.221.0.221.0.26
EIPPlaceHolderNANANANA1.0.91.0.181.0.221.0.221.0.221.0.221.0.26
EdgeIO DTMNANANANANANANANANANA1.1.25092.10

(*) Version 1.0.38 in V16.0.12192, and version 1.0.41 in V16.0.01261