How can we help you today?

Serial Port Pin-Out for SAGE RTU 2400

Issue:

Users need the correct pin-out configuration for the DB-9 serial ports on the SAGE RTU 2400 for connecting external devices or troubleshooting communication issues.

Product:

SAGE RTU 2400

Environment:

  • SAGE RTU 2400 Baseboard
  • Optional C3438 RS-232 Port Card
  • SCADA communication setup using RS-232 serial ports

Cause:

Incorrect wiring or misunderstanding of the DB-9 connector pin assignments can lead to communication failures between the RTU and external devices such as IEDs, MTUs, or modems.

Resolution:

The SAGE RTU 2400 baseboard provides five serial ports:

  • UIF Port (dedicated for PPP or Console)
  • Ports 1–4 (for communication with IEDs, MTUs, or redundant channels)
    Additional ports (up to 12 total) can be added using C3437/C3438 expansion cards.

DB-9 Pin-Out Configuration:

1

For basic RS-232 communication, only pins 2 (RXD), 3 (TXD), and 5 (GND) are required. Other pins are used for modem control and synchronous connections.

LED indicators on the baseboard show activity for DCD, RX, RTS, TX, CTS for each channel.

Schneider Electric Nigeria