How can we help you today?

What is Included in the SAGE RTU CPU Upgrade Kit?

Issue

Users need to know the components and part numbers provided in the CPU upgrade kit "C3414-KIT-800S2" for upgrading SAGE RTU units to the C3414 CPU.

Product

SAGE RTU Product Line (models supporting C3414 CPU upgrade)

Spare part number C3414-KIT-800S2

Environment

Utility substations or industrial automation systems where SAGE RTUs require CPU upgrades for performance improvements or firmware compatibility.

Cause

Upgrading the CPU is necessary to support newer secure firmware versions, enhanced features, or replace obsolete hardware.

Resolution

The C3414 CPU Upgrade Kit (C3414-KIT-800S2) includes the following components:

Part Number

Description

Qty

C3414-000-00001

PCA CPU LX800 with Compact Flash & Firmware

1

C3413-CB1-00007

Ribbon Cable Assembly (Flat FF 50/100F0)

1

B0000-079-11500

Ethernet Cable 10Base-T, 15 ft

1

J4001-242-00000

Machine Screw 4-40 BH SS

4

J0203-185-00000

Internal Lock Washer No. 3 SS

4

Important Notes:

  • Back up your existing configuration before replacing the CPU.
  • Use the Configuration Conversion tool to ensure compatibility with the new CPU.
  • Do not remove the ribbon cable once installed.

Schneider Electric Nigeria