Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Compact DEP217/218 to X80 DAI1602/1604 quick wiring - 990XSM00201

Issue

Migrating an ASBDEP217/218 to a BMXDAI1602/1604 and need to confirm the 990XSM00201 quick wiring cable pinout.

Product line

Modicon X80, M340, M580

Resolution

Below is an image of the pinout.

wiring pinout

Schneider Electric Nigeria

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: