Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Why Unity Variable Management tool is not working properly in Control Expert 16.2 ?

Issue

Need of import/export .xsy file in an EcoStruxure Control Expert Version 16.2 application either :

  • Containing arrays with predefined values.
  • Related to M580 Safety.

Product Line

EcoStruxure Control Expert 16.2, applicable to Modicon M340, M580, and other supported PLC platforms.

Resolution

To resolve this issue, please use Unity Variable Management tool embedded in EcoStruxure Control Expert Version 16.0, also attached in this FAQ.

Schneider Electric Nigeria

Attachment(s)
Unity Variables Management.xlsm [865 KB]
Variables Management Using Microsoft Excel.pdf [1.25 MB]