Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Operation Modes of PowerLogic A3 Arc Flash Protection Relay

Article available in these languages: Spanish

Issue:
What are the different operation modes of PowerLogic A3 and when should each be used?

Product:
PowerLogic A3 Arc Flash Protection Relay

Model A3F6P

Model A3F12P

Model A3S6P

Model A3S12P

Environment:
Medium- and low-voltage switchgear installations requiring arc flash protection.

Cause:
Users need to understand the flexibility of PowerLogic A3 for various system architectures and selectivity requirements.

Resolution:
PowerLogic A3 supports three operation modes:

  1. Stand-alone Mode
    • Used for simple systems with a single A3F device (full size with power supply).
    • Provides independent protection using light-only criteria.
    • Example: A3F6P or A3F12P installed in incomer or feeder cubicle.
  2. System Mode
    • Up to 5 A3 devices connected via ArcEM cables.
    • Allows sharing of sensor data and commands across devices.
    • Supports selective and non-selective schemes for multi-bay systems.
    • Limitations: Total cable length ≤ 100 m; max distance between devices = 30 m.
  3. I/O Peripheral Mode
    • Integrates with V321 central unit for advanced arc protection.
    • Up to 16 A3 devices can be cascaded.
    • Enables complex schemes with current confirmation and IEC 61850/Modbus communication.

Key Considerations:

  • Use stand-alone mode for single cubicle protection.
  • Use system mode for small switchgear with multiple feeders.
  • Use I/O peripheral mode for large installations requiring SCADA integration and advanced logic.

Schneider Electric Nigeria

Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: