Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to Start a Can-Open slave with the master BMECXM0100?

Title

How to Monitor and Change a CANopen Slave Status from STOP to OPERATIONAL Using Application Logic.

Question

The goal of this FAQ is to explain how to monitor and transition a CanOpen slave device from STOP to OPERATIONAL mode using the application logic.

Answer

1. Issue

The goal of this FAQ is to monitor the status of a CANopen slave device and, if it is in STOP mode, change its state to OPERATIONAL mode using the application logic.

2. Product Line

Hardware: BMECXM0100 (CANopen Master)
Relevant objects: Slave DDT object HEALTH
NMT commands and Write_SDO EF functionality are used for state control.

3. Environment

  • Operating System: Windows 11
  • Software: EcoStruxure Control Expert (or equivalent), supporting CANopen communication
  • Communication: CANopen protocol with NMT state machine and SDO commands

4. Resolution

  • Monitoring Slave Status:

The status of each slave is available in its DDT under the object named "HEALTH".

image30

  • Health Parameter:

The table below describes the meaning of each value for the HEALTH parameter:

image31

Example: If the Health byte equals 6, the slave is in Operational mode.

  • Changing the Slave State:

If a CANopen slave connected to a BMECXM0100 master is in STOP mode, you can send an NMT=H05 command to force it into Operational mode.

Below is a diagram of the NMT State Machine and the list of available NMT commands:

image32

This NMT command can be send by the application logic, using a WRITE_SDO communication EF.

  • How to Use WRITE_SDO:

Here's a detailed explanation:

image33

      • SUBINDEX: Address of the target slave (e.g., @3 in this example)
      • NODE:  Must contain 127 (represents the sending device, the CXM)
      • INDEX: Must contain the NMT command encoding 16#1F82.
      • DATA_IN: Must contain the NMT command value, e.g., H05 for Operational mode
      • In the application, the variable SDO_DATA_TO_WRITE is a 49-byte unlocated array.

        image35

      • Here is an excerpt from an animation table that sends command 05 to move the slave into in Operational mode:

        image36

    • The EF is triggered when the input start_single_CMD = 1.
    • Note: Entering 16#04 will put the slave into STOP mode.

  • Attached are:
    • The section for using the Write_SDO EF to control a slave.
    • The section for enabling the Write_SDO query.

5. FAQ Applicable Conditions (Optional)

This procedure applies to BMECXM0100 masters controlling CANopen slaves. It remains valid until firmware updates introduce alternative methods for state control.

Schneider Electric Nigeria

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: