How the "broken wire" option on X80 analog input modules works?
Issue:
How to use the "broken wire "option embedde in X80 analog module ? (Example using BMXART0814 analog input module ).
Product Line:
X80 analog modules with "broken wire" option available
Environment:
EcoStruxure Control Expert, Windows 10
Resolution:
Example using the BMXART0814 analog input module with the 'Broken Wire Test' enabled:
If one of the input wires becomes broken or disconnected, the fault can be detected using one of the following methods:
-
The module's 'ERR' LED will turn red, and the corresponding channel LED will blink to indicate the fault:
- The faulty channel will be displayed in the Debug view of the module:
- If the "READ_STS" FFB is used in the plc program, It will provide more details on the IODDT:
Using with the T_ANA_IN_T_BMX device DDT configured:
Using the T_U_ANA_TEMP_IN_8 device DDT configured:
Released for: Schneider Electric Nigeria