Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
FGEN Obsolescence and Alternative Random Number Function Block for SCADAPack

FGEN Function Block Status

  • FGEN is obsolete in Control Expert and was not migrated to RemoteConnect Logic Editor or SCADAPack, as it originates from an outdated library.
  • While still available as a standalone in Control Expert 16.2, it is not supported with RemoteConnect to avoid legacy practices.

Alternative

  • Use a derived function block (shared for reference only) to generate random numbers.

Derived Block Features

  • Generates random numbers within a specified range.
  • Output type: Integer or Float (only one active at a time).
  • Range limits:
    • Integer: LowLimit to HighLimit
    • Float: FloatLowLimit to FloatHighLimit
  • Selection:
    • floatout = 0 → Integer output
    • floatout ≠ 0 → Float output
Random Generator

Schneider Electric Nigeria

Attachment(s)
GenerateRandom.zip [2 KB]