How can we help you today?

How do I create a new switchboard in EcoSet Config?

To create a new switchboard, do the following:

  1. Click Create a switchboard under List view.
  2. Update the following fields under the ELECTRICAL CHARACTERISTICS

section:

    • Switchboard name: * Enter a name for the switchboard.
    • Rated current - In [A]:Enter the rated current value.
    • Short circuit current - Isc [kA]: Enter the short circuit current value for Isc1 (single phase short circuit intensity) and Isc3 (three phase short circuit intensity) value.
  1. Click Create.

Note: Fields marked with (*) are mandatory to fill.

You can create multiple switchboards in the same project using the steps mentioned above. After creating a switchboard, you can:

    • Easily organize the electrical network by selecting switchgear.
    • Save configurations for future use.
    • Use the Duplicate option to re-use switchgears, speeding up switchboard configuration.

Create a New Switchboard
switchboard creation

Schneider Electric Nigeria