How can we help you today?

Can't configure IEC61850 in P30

Issue

Recently we received some BFO cases where customer don’t know how to configure IEC61850 in P30 relay.

11

_____________________________________________________________

Product Line

P30

_____________________________________________________________

Environment

All firmware

_____________________________________________________________

Phenomenon

MCL 61850 and CID 61850 Folder are grey color and can’t be configured.

_____________________________________________________________

Root Cause

It is needed to enable IEC61850 ed1 or ed2 first and refresh the connection.

_____________________________________________________________

Solution

Enable IEC61850 ed1 or ed2 first.

1

Then refresh the connection.

2

Then we will see MCL61850(ed1) or CID61850(ed2) folder is ready for configuration.

3

Schneider Electric Nigeria
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings