How can we help you today?

How do I organize a switchgear in EcoSet Config.

As a panel builder, using EcoSet Config, you arrange selected switchgears to form an electrical network. By dragging and dropping products to establish a hierarchy, you create an electrical network.

Ensure that the first product in the electrical diagram is already in place. The main incomer product cannot be removed from the diagram but can be replaced with a transfer switch if necessary, refer to section (A).

  • Use the expand icon + to expand the hierarchy.
  • Use the collapse icon - to collapse the hierarchy.

You can access the list of product catalogue on the left side of the panel. To organize a switchgear, follow the steps mentioned below:

  1. To add the product role card in the diagram, drag them to the Add + icon and release when they are added.
  2. To duplicate the product role cards in the diagram, click More : > Duplicate.
  3. To delete a product, click More : > Delete.

You can view and validate the electrical network in Single Line Diagram tab.

Organize a Switchgear

Image

Schneider Electric Nigeria