Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Understanding Input Fast Fault on Symmetra MW UPS: Causes and System Response

Introduction

This document explains the Input Fast Fault alarm on Symmetra MW UPS systems, detailing its triggers, system response, and recommended troubleshooting steps.


Detailed Explanation

The Input Fast Fault alarm occurs when the UPS detects a severe and rapid abnormal condition on the incoming AC supply. The system reacts almost instantly to protect its rectifier, inverter, and connected loads.

Common Triggers

  1. Severe Voltage Deviation
    Input voltage rises or drops outside the UPS tolerance window (often ±15–20% of nominal).
    Example: Utility sag/surge or upstream breaker operation.

  2. Phase Loss or Phase Reversal
    One or more input phases disappear or swap positions, often caused by wiring errors or upstream breaker trips.

  3. Frequency Out of Range
    Input frequency changes rapidly beyond limits (e.g., ±3 Hz from nominal), common during generator synchronization or unstable utility.

  4. High Harmonic Distortion or Transients
    Large spikes or electrical noise on the input line, usually from switching large inductive loads or upstream faults.

  5. Input Source Instability
    Rapid fluctuations in voltage or frequency that the UPS cannot track, happens during generator startup or source transfers.

  6. Breaker or Fuse Issues
    Loose connections or blown fuses causing intermittent phase loss.


System Reaction

When an Input Fast Fault occurs:

  • The UPS disconnects from the input immediately.
  • Transfers to battery or bypass depending on configuration.
  • Alarm remains active until input stabilizes and the UPS re-synchronizes.

Recommended Troubleshooting Steps

  • Verify input voltage and frequency are within acceptable limits.
  • Check upstream breakers and fuses for proper operation and tight connections.
  • Inspect for phase loss or reversal in the input wiring.
  • Monitor for harmonic distortion or transient events on the input source.
  • If using a generator, ensure proper synchronization and stable output before switching to UPS input.
  • Review event logs for repeated occurrences and consult manufacturer support if the issue persists.