How can we help you today?

How many syslog messages could be stored in the local buffer of the BMECRA31310(H) ?

Issue

How many syslog messages could be stored in the local buffer of the BMECRA31310(H) ?

Product Line

M580

Environment

Control Expert 16.2

Resolution

Up to 2048 event messages are stored in the local buffer of the BMECRA31310(H) adapter module. The oldest buffer will be overritted by new arrival events when the buffer is full.

Schneider Electric Nigeria

Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings