Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to use the scheduler task in EcoStruxure Machine SCADA Expert v2023?

Article available in these languages: Spanish

Issue:

The Scheduler is used to execute program logic (using the Built-in Scripting Language) at a specific date/time, on a certain time interval, at the occurrence of a defined event.

In this FAQ an example using the Clock event type is shown.

Product:

EcoStruxure Machine SCADA Expert v2020, v2023

Environment:

HMI Configuration Software in Windows

Resolution:

The Scheduler worksheet consist of the following columns:

Event: There are three types of events: Calendar, Clock, and Change.

  • Calendar: Events that occur on time bases greater than 24 hours (e.g., print a report every Friday at a certain time).
  • Clock: Events that occur on time bases smaller than 24 hours (e.g., intervals in minutes or seconds).
  • Change: Events related to a change in a tag defined in the Trigger field.

Trigger: Used only with the Change event. When the tag defined here changes, the Expression will be evaluated.

Time: Used with the Calendar and Clock event types.

  • With Calendar, when the specified date and time occurs, the Expression will be evaluated.
  • With Clock, the Expression is evaluated based on the time interval configured in Time, starting from when the project begins running.

Type a time using the HH:MM:SS.ms format. Valid values are:

  • Hours: 00 to 23
  • Minutes: 00 to 59
  • Seconds: 00 to 59
  • Milliseconds: 1 to 9 (optional)

Examples:

  • 03:00:00 = every three hours
  • 00:00:00.1 = every 100 milliseconds

Date: Used only with the Calendar event type.

The order and separator settings determine the overall date format.

For example:

  • Default: MM/DD/YYYY (e.g., 02/13/2015)
  • ISO 8601: YYYY-MM-DD (e.g., 2015-02-13)

Tag: The tag that will receive the value returned from the Expression.

Expression: The expression to be evaluated.

Disable: Condition to disable the event.

Example using the Clock event.

1

Adding the tag to the Output window log:

2

3

Result:

4

Note: Really close to the 100ms defined; for larger intervals, this will be more precise.

Related resources:

Title: EcoStruxure™ Machine SCADA Expert, Help Manual

URL: https://download.schneider-electric.com/files?p_Doc_Ref=EIO0000002448&p_enDocType=User+guide&access=Public

Relevant Pages:

  • Page 502: Time format details
  • Page 680: Date format details