How to print the logic of a project in Control Expert?
Issue:
This FAQ explains the steps to print the project logic and provides tips for better organization.
Product:
EcoStruxure Control Expert (previously Unity Pro)
Environment:
PLC Configuration Software in Windows
Resolution:
To print the logic to a PDF, follow the steps shown in the image below:
Note: You can select which sections you want to print. In this example, all sections were selected.
Unfortunately, we are limited to a certain number of columns and rows (space) per page type. You can adjust the page setup and margins to fit as much of the logic as possible:
You can also enable Page Breaks to view how each page is divided. This feature helps you understand what content will appear on each page:
These are the available features you can use when working with the project printout.
Released for: Schneider Electric Nigeria