How can we help you today?

Is EcoStruxure Machine SCADA Expert v2023 compatible with the HMIG5U21?

Issue:

Can Machine SCADA Expert v2023 run correctly in the Harmony GTU HMI open box HMIG5U21?

Product:

  1. EcoStruxure Machine SCADA Expert v2023
  2. HMIG5U21

Environment:

  1. HMI Configuration Software in Windows
  2. Harmony GTU HMI open box with Windows 10 IoT

Resolution:

Short answer: In theory it is compatible but it is not recommended.

EcoStruxure Machine SCADA Expert v2023 have the following requirements:

From: EcoStruxure™ Machine SCADA Expert , Help Manual - 07/2024 - P.38

1

The HMIG5U21 barely meets these requirements:

From: HMIG5U21 product data sheet

2

Note: Keep on mind that the actual available memory might be less than 4 GB, especially if the OS and other tasks are running.

From: Harmony GTU, User Manual - 01/2022 - P.12

3

The HMIG5U21 is theoretically compatible with EcoStruxure Machine SCADA Expert v2023; however, it is not recommended for Machine SCADA Expert applications. Machine SCADA Expert projects are typically complex and may require even more system resources.

Related resources:

Title: EcoStruxure™ Machine SCADA Expert, Help Manual

URL: https://download.schneider-electric.com/files?p_Doc_Ref=EIO0000002448&p_enDocType=User+guide&access=Public

Title => "Harmony GTU, User Manual"

URL => https://download.schneider-electric.com/files?p_Doc_Ref=EIO0000001735&p_enDocType=User+guide&access=Public

Schneider Electric Nigeria