How can we help you today?

What are the password requirements for Power Monitoring Expert applications?

Issue

Need to know what restrictions are applied to the supervisor password for PME during new installations or upon resetting the password.

Product Line

Power Monitoring Expert 2024

Power Monitoring Expert 2023

Power Monitoring Expert 2022

Power Monitoring Expert 2021

Environment

PME Fresh Install

PME Reset Accounts Tool

Cause

Power Monitoring Expert has introduced a minimum password requirement when creating the supervisor account on the system. If this requirement is not met, the process may fail or introduce errors later in the system.

Resolution

Minimum Password Length - Needs to be at least 8 characters but best practice recommends 14+ characters

Character Type - Must contain a mix of uppercase letters, lowercase letters, numbers, and symbols

Password Reqs

Schneider Electric Nigeria