How can we help you today?

Easy-UPS Li-ion 1-3kVA - NMC Reports Cell Overvoltage on the Battery Pack

Note: This is only for the Easy-UPS Li-ion 1-3kVA. For the Easy-UPS Li-ion 6kVA please go to this FAQ.

Problem:

The NMC web interface reports a battery pack cell overvoltage.

Battery cell overvoltage

Answer:

To stop this alarm from showing on the NMC, the firmware on the NMC must be upgraded to the latest version and the battery pack firmware must be upgraded. Please see the attachments for the battery pack firmware upgrade process, the required software and the firmware file.

Schneider Electric Nigeria

Attachment(s)
Easy-UPS Li-ion 1-3kVA Battery Firmware.zip [1.33 MB]