How can we help you today?

How to operate the AR8132A APC by SE Combination Lock Handles?

Question:
How to operate the AR8132A APC by SE Combination Lock Handles?

Product:
AR8132A

Environment:

All serial numbers

Answer:

Parts Identification:

The following is an image showing the parts of a Combination Lock Handle

  1. Unlock using the Dials: (NOTE: The use of the provided key 222 will override the combination)
    The following image shows an AR8132A with the Key
    1. Dial the current combination (1) (The factory default is “000”).
    2. Turn the wing knob (3) until the arrow (2) points up (unlocked position).
    3. The handle can then be lifted up and swung to unlock the door.
      The following image shows an unlocked combination lock handle
  2. Lock using the Dials:
    1. Turn the wing knob (3) until the arrow (2) points down (locked position).
    2. Turn the dials (1) to randomize dials and clear the combination.
  1. Changing the Combination: (NOTE: To change the combination, the existing combination must be known. If lost, please refer to FA164019)
    1. Dial the combination (1). The factory default is “000”.
    2. Turn the wing knob (3) until the arrow (2) points up (unlocked position).
    3. Turn it counterclockwise an additional 15°, and enter desired new combination.
      The following image shows how the knob should be turned in order to unlock the combination lock handle
    4. Turn the wing knob clockwise 15° back to the unlocked position. The new combination is set.

Schneider Electric Nigeria

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings