Easy-UPS Li-ion 6kVA - NMC Reports Cell Overvoltage on the Battery Pack
Note: This is only for the Easy-UPS Li-ion 6kVA. For the Easy-UPS Li-ion 1-3kVA please go to this FAQ.
Problem:
The NMC web interface reports a battery pack cell overvoltage.
Answer:
To stop this alarm from showing on the NMC, the firmware on the NMC must be upgraded to the latest version and the battery pack firmware must be upgraded. Please see the attachments for the battery pack firmware upgrade process, the required software and the firmware file.
Released for: Schneider Electric Nigeria