How to Power cycle an InRow Cooling Unit Gen2?
PUBLIC
Issue:
How to Power cycle an InRow Cooling Unit Gen2?
Product Line:
InRow Family Gen2.
Environment:
ACRD3XX, ACRC3XX, ACRH3XX, ACRD6XX, ACRC6XX, UNIFLAIR SP, etc.
Cause:
General aid for Customers
Resolution:
- Please click on the home icon (Fig 1) 👇🏻
Figure 1
- Click on the On/Off button (Fig 2), you might be required to input the pin, use the default one: 1234.
Figure 2
- Change the state from on to off (Or StandBy), then click OK (Fig 3).
Figure 3
- When the fans start ramping down, please unplug the dedicated power cord(s) to the unit (It can be top or bottom fed) [Figure 4] or put down the dedicated breaker(s) to the unit (If it’s hard-wired), or if it’s a 600mm InRow (Figure 5) and leave the unit without any power for at least 5 minutes.
Figure 4 (For 300mm InRow only).
Figure 5 (For 600mm InRow only).
- After the 5 min passes, restore the power to the unit, allow a couple of minutes, for the display to pop up, change the mode from Off to On (Figure 3), and test the proper operation of the unit.
NOTE: This process can only be executed from the front display of the unit.
Released for: Schneider Electric Nigeria