How to open the hardware configuration on a HMI programmed with EOTE?
Issue
It is not clear how to open the hardware configuration on a physical HMI programmed with EcoStruxture Operator Terminal Expert
Product Line
EcoStruxture Operator Terminal Expert
HMI running EOTE, EOTE Runtime
Resolution
There are 2 options to try and open the hardware configuration on an HMI running EOTE
[Option 1]
Display with Touch Gestures
Within 0.5 seconds, touch the top-right then bottom-left corners, or the top-left and bottom-right corners (within a 40 pixel area) of the screen
This option can be enabled / disabled from the settings as follows.
1/ In the Project Explorer window, from [System Architecture] click [Target01].
2/ In the Properties window, go to [Function] tab ➞ [Options] tab ➞ [Preference].
[Option 2]
Display with Hardware Configuration object on a screen
Note: The size of the object is the size of the Hardware Configuration screen. It is not a button.
If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.
If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)
Released for: Schneider Electric Nigeria