How can we help you today?

Reports Time Out In PME Web Apps

Issue

When running reports, the report will timeout with an error:

"An error occurred while attempting to retrieve the data."

Errors

Product Line

Power Monitoring Expert 2022

Power Monitoring Expert 2023

Power Monitoring Expert 2024

Environment

Web Applications Reports

Management Console

Cause

Report querying is dependent on multiple factors (number of source measurement pairs, resources available to SQL, number of simultaneous sessions, etc). Some reports may require additional time than the standard 5 minutes.


Resolution 1

  1. Navigate to Management Console -> Tools -> Reports Configuration.
  2. Increase timeout seconds.

Report Subscription

**Note that increasing timeout may cause reduced performance**

Resolution 2

Warning: Irreparable database damage can occur. This procedure should only be performed by users familiar with SQL Server Management Studio. Databases should be backed up prior to performing this procedure.

If the above does not work, the following locations can be edited to increase timeout.

SELECT TOP (1000) [Module]

,[Category]

,[Item]

,[Value]

,[DefaultValue]

FROM [ION_Network].[dbo].[vCFG_ConfigItems]

where item like '%timeout%'

Reports

Setting a maximum time of 1800 seconds (30 mins) for these fields may allow the report to complete. Please contact support prior to making these changes.

Schneider Electric Nigeria
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings