How can we help you today?

Why am I getting a .NET framework 3.5 service pack 1 error during installation of Control Expert 16.2?

Issue:

Why am I getting a .NET framework 3.5 service pack 1 error during installation of Control Expert 16.2?

Product Line:

Control Expert

Resolution:

control expert 16.2 .net framework 3.5 error

First make sure the .NET framework is installed and active on your machine

Method 1 — Check via Windows Features

  1. Press Windows Key + R
  2. Type:
  3. Optional features
  4. Press Enter
  5. In the Windows Features window, look for:
    • “.NET Framework 3.5 (includes .NET 2.0 and 3.0)”
  6. Status meanings:
    • Checked → Installed
    • Unchecked → Not installed
    • Filled box → Partially installed

Method 2- Check using Command Prompt

  1. Open Command Prompt

  2. Run this command:

    BAT
    reg query "HKLM\SOFTWARE\Microsoft\NET Framework Setup\NDP\v3.5"

If .NET 3.5 is installed, you will see a Version entry like:

Version    REG_SZ    3.5.30729
If it says "The system was unable to find the specified registry key" → It’s not installed.


Method 3- PowerShell Command

Open PowerShell and run:

PowerShell
Get-WindowsFeature Net-Framework-Core

Look for:

  • Installed → It’s on your system
  • Available → Not installed, but can be enabled

Method 4- Check the File System

Look for this folder:

C:\Windows\Microsoft.NET\Framework\v3.5\

If the folder exists → .NET 3.5 is installed.

 

If it is not installed please go to the windows site here:

https://www.microsoft.com/en-ca/download/details.aspx?id=25150

If it is unchecked, please check it. It might ask permission to update and download new files to complete the installation. Please allow it

After it is done, reboot and check the feature again.

control expert 16.2 .net framework update error

Now you should be able to install the software with no further issues

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)

Schneider Electric Nigeria
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
Start your sales enquiry online and an expert will connect with you.

Where to buy?

Where to buy?

Easily find the nearest Schneider Electric distributor in your location.

Help Centre

Help Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings