How can we help you today?

How do I perform the initial internal battery connection? | Back UPS PRO RS/NS M2, MS & Gaming UPS (BGM series)

Issue:

The Back UPS PRO RS/NS M2, MS & Gaming UPS (BGM series) does not power on or begin charging when first connected.

Product Line:

Back UPS PRO RS/NS M2, MS & Gaming UPS (BGM series)

Environment

BR1000MS, BN1100M2, BR1350MS, BN1350M2, BN1375M2, BN1500M2, BR1500MS, BGM2200-MSX / All serial

Cause:

When purchasing a UPS from the Back UPS PRO RS/NS M2 ,MS & Gaming UPS (BGM) family, it is necessary to perform the initial connection of the internal battery before operating the unit. If this step is skipped, the UPS will not function properly or begin charging its batteries.

Resolution:

See the procedures:

Connect 1

Connect 2

Please see the link below and the attached video.

Schneider Electric Nigeria

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings