How can we help you today?

How to delete old archive links from Archive Manager in Ecostruxure Automation Expert

This knowledge base article explains User on how to delete unwanted archive links deployed to Archive Manager in Ecostruxure Automation Expert.

In this example, we have two archive links where one is running and active, another one is not running needed to be removed.

ar1

For deleting the archive link, Open Archive Manager and select the link which needs to be deleted as shown in the above picture.

ar2

We need to login first, in order to get access to delete the archive link. Click on Login.

ar3

Provide the credentials as Username: managementservice and Password: managementservice. User will able to login and option for delete will be enabled.

ar4

Click on Delete and the archive link shall be deleted after giving confirmation to the popup provided.

ar6

This is the process for deleting the archive links from Archive manager. This is applicable for all versions of Ecostruxure Automation Expert Softwares.