How can we help you today?

PME - How to add software logging for individual circuits on a native multi-circuit device type using Device Type Editor

Product Line

Power Monitoring Expert 9.0

Power Monitoring Expert 2020

Power Monitoring Expert 2021

Power Monitoring Expert 2022

Power Monitoring Expert 2023

Power Monitoring Expert 2024

Environment

Device Type Editor

Resolution

Note: This procedure assumes the individual circuits are configured in the device type using the !!DeviceName_M##!! format. The example steps below configure software logging for Active Power for the circuits in the native EM4800-08 Wye device type:

1. Open File Explorer, then navigate to …\Program Files (x86)\Schneider Electric\Power Monitoring Expert\system\translators:

2. Copy the em4800_08_wye.ion and em4800_08_wye.xml files:

system translators .ion and .xml files

3. In File Explorer, navigate to …\Program Files (x86)\Schneider Electric\Power Monitoring Expert\config\translators.

4. Paste the em4800_08_wye.ion and em4800_08_wye.xml files into this folder:

Pasted files in config translators

5. Open Management Console > Tools > System > Device Type Editor:

Device Type Editor

6. File > Open, then navigate to …\Power Monitoring Expert\config\translators:

Open config translators

7. Open the em4800_08_wye.ion file.

8. In Device Type Editor, open Tools > Configure Software Logging:

Configure software logging

9. Highlight each of the Real Power Total!!DeviceName!!_M0# measurements, then check the box for Log:

Check box for log on individual circuits

10. Click OK to close the window, then File > Save.

Schneider Electric Nigeria