How can we help you today?

PME - How to expose measurements to OPC server using Device Type Editor

Product Line

Power Monitoring Expert 9.0

Power Monitoring Expert 2020

Power Monitoring Expert 2021

Power Monitoring Expert 2022

Power Monitoring Expert 2023

Power Monitoring Expert 2024

Environment

Device Type Editor

Resolution

Note: There isn't a way to open a previously exported .xml with OPC Selector in Device Type Editor. If you want to expose additional measurements after following this procedure once, you'll need to reselect all of the measurements you want to expose, then replace the file in the …\Program Files (x86)\Schneider Electric\Power Monitoring Expert\system\IONServices\DefaultMeasurementsExt folder each time.

1. Open Management Console > Tools > System > Device Type Editor:

2. File > Open, then navigate to …\Power Monitoring Expert\config\translators:

config translators

3. Open the .ion file for the device type you want to expose measurements to the OPC server.

4. Open Tools > Expose OPC Measurements.

5. Select a measurement, then click the >> button to move it to the right pane. Repeat for the remaining desired measurements.

OPC Selector

6. Click Save.

7. Navigate to …\Program Files (x86)\Schneider Electric\Power Monitoring Expert\system\IONServices\DefaultMeasurementsExt.

8. Save the file in this folder.

  • Note: You may get a permissions error. If so, save the file to your Desktop or another location then copy/paste it into the …\Program Files (x86)\Schneider Electric\Power Monitoring Expert\system\IONServices\DefaultMeasurementsExt folder.

9. Open File Explorer and confirm the exported file is saved to the folder:

DefaultMeasurements file

10. Navigate to …\Program Files (x86)\Schneider Electric\Power Monitoring Expert\config\IONServices, then make a copy of the IONServicesConfiguration.xml file to have as a backup. If this folder doesn’t exist, skip this step:

Backup the OPC server configuration

11. Open Management Console > Tools > System > select Update OPC Server.

Schneider Electric Nigeria
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
Start your sales enquiry online and an expert will connect with you.

Where to buy?

Where to buy?

Easily find the nearest Schneider Electric distributor in your location.

Help Centre

Help Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings