How can we help you today?

How to Switch between Map View and Table View on the SmartConnect Dashboard

Issue:

Users may want to switch between the Map View and Table View options on the Dashboard of their SmartConnect Portal.

Product Line

SmartConnect Portal

Cause

A recent update of the SmartConnect application now shows the Map view in the Dashboard UI by default.

Resolution

There is a toggle in the UI that allows users to switch between the Map view and the Table View. This toggle information is saved so the users view preference should persist between sessions.

1

Schneider Electric Nigeria
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings