How can we help you today?

Can you program an M221 controller through the Modbus Serial Port?

The serial interface of a M221 controller is strictly for field communication protocols (e.g., Modbus RTU) and not to connect with Machine Expert Basic.
The communication with Machine Expert Basic is available only via the Ethernet or USB ports.

Schneider Electric Nigeria
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings