How can we help you today?

What is the cause of the FWPF error on an ATS480?

Issue:

What are the possible causes of an FWPF error on an ATS480?

Product Line:

ATS480

Environment:

Display shown on the VW3A1111 keypad

Resolution:

If the ATS480 is powered on with the VW3A1111 keypad and it displays a FWPF fault, with the soft starter powered off, remove the VW3A1111 keypad and connect the mini keypad that comes with the unit. Then power it back on and press OK to clear the fault.

Schneider Electric Nigeria

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings