How can we help you today?

How to change the output voltage of 120Vac Single Phase Smart UPS?

Issue: How to change the output voltage of 120Vac Single Phase Smart UPS?


Product Line:
Smart-UPS Line Interactive


Environment:
SMC, SMX, SMT, SMTL with 110, 120 and 127 V capability output settings, all serial numbers

Regions like Mexico generally uses a residential voltage of 127 V, while Jamaica uses 110 V phase voltage.


Resolution


APC by Schneider Electric recognizes this and made it possible for other regions like Mexico and Jamaica to use our products by configuring the output voltage settings to either 110, 120 or 127 V. Please see instructions below on how to change the output voltage settings on the LCD display of the UPS.



To change output voltage settings on SMC models, we need to enter on Configuration mode. Hold the MUTE and MENU buttons together for 2 seconds until the system emits a short beep and the display will flash to indicate the UPS has entered Configuration Mode. When in Configuration Mode, press the MENU button to cycles the display through the available options and search for Out 120V. Press on the MUTE button and select the desired output voltage (not available on some models).


To change output voltage settings on SMT, SMX models, we need to change the Menu type to Advanced. Go to Configuration then select Menu Type and set it to Advanced. Go back to Configuration then select Output voltage and select the desired Output voltage configuration.



To change output voltage settings on SMTL models, we need to change the Menu type to Advanced. Go to Config Menu then select Display and go to Menu type and change it to Advanced. Go back to Config Menu and select Low or High Transfer, then select the desired output.

For those units above with a network card, we can change it under Configuration Menu then select Power Settings and select the Rated Output Voltage. Kindly see below reference:

Picture of the web GUI showing the Power Settings


Should there be any other questions and/or concerns, feel free to reach out to us at 1-800-800-4272 or our chat with our technical support group atAPC by Schneider Electric Customer Technical Support

Schneider Electric Nigeria
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
Start your sales enquiry online and an expert will connect with you.

Where to buy?

Where to buy?

Easily find the nearest Schneider Electric distributor in your location.

Help Centre

Help Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings