How can we help you today?

PowerChute Network Shutdown Linux Virtual Machine has been flagged for CVE-2026-31431, CVE-2026-43284, CVE-2026-53266, CVE-2026-98432, CVE-2026-111497

Issue:

The PowerChute Network Shutdown Linux Virtual Machine has been flagged for CVE-2026-31431, CVE-2026-43284, CVE-2026-53266, CVE-2026-98432, and CVE-2026-111497

Product:

PowerChute Network Shutdown

Environment:

PowerChute Network Shutdown Linux Virtual Machine.

Cause:

https://nvd.nist.gov/vuln/detail/CVE-2026-31431

https://nvd.nist.gov/vuln/detail/CVE-2026-43284

https://nvd.nist.gov/vuln/detail/cve-2026-53266

https://nvd.nist.gov/vuln/detail/cve-2026-98432

https://nvd.nist.gov/vuln/detail/cve-2026-111497

Solution:

Update the Linux system as recommended in the PowerChute Network Shutdown Security Handbook and Installation Guide.

1- To update the system log in to the PowerChute Linux VM as root and run the command dnf update.

dnf update command

2- When the command runs, you will be prompted to accept the update. Note that the update installation packages and upgrade packages will vary.

Answer yes or no

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: