How can we help you today?

How to resolve the issue of being unable to uninstall SE License Manager from the Control Panel

Customer cannot uninstall SE license Manger from Control Panel with error message.

error msg

You can try the following method:

  • Press Win + R, type regedit, then right-click Registry Editor and select Run as administrator.
  • Navigate to the following path:
  • HKEY_CLASSES_ROOT\Installer\Products
  • From the top menu, click Edit → Find, then search for: Schneider Electric License Manager
  • After locating the matching registry key, look in the right-hand pane for a string value named Transforms.
  • Double-click Transforms, delete the entire path shown in the Value data field so that it is left blank, then click OK.
  • Close Registry Editor, go back to the installed programs list, and try uninstalling the License Manager again.

Schneider Electric Nigeria
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings