How can we help you today?

Video: Setting up the Edge IO with Machine Expert V2.3 and a M262 using Ethernet/IP protocol

Issue:

Setting up the Edge IO with Machine Expert V2.3 and a M262 using Ethernet/IP protocol.

Product Line:

Edge IO, Machine Expert, M262 PLC

Resolution:

Please see video for configuration

Hardware:

TM262M35MESS8T

M262 Controller

NTSNEC1200

Edge I/O - Network Interface Module Ethernet/IP, Modbus/TCP

NTSPFB1002H

Edge I/O Power Supply Module

NTSDDI1602X

Edge I/O – Discrete Input Module, 16 In

NTSDDO0802

Edge I/O – Discrete Output Module 8 Out

NTSAMI0400

Edge I/O – Analog Input 4 In

NTXAMO0400

Edge I/O – Analog Output 4 Out

  1. Creating a BOM using the Configuration tool
  2. Connecting to the Web Server of the Edge I/O
  3. Mapping the Edge I/O modules with Machine Expert V2.3
  4. Mapping through the EDS file.
  5. EcoStruxure Automation Device Maintenance Tool (EADM)

Default User: SecurityAdmin

Default Password: AAAAAAAA

Default IP address: 10.10.X.X, where the last two octets are derived from the MAC address (converted from hexadecimal to decimal).

00:00:54:C8:05:83 à 10.10.5.131

switches

Rotary Switch Settings

TENS (x)

ONES (y)

Mode

Description

0–15

0–9

DHCP

Enables DHCP for automatic IP assignment. Allows device naming for DHCP/FDR server.

Format: DeviceName_TensOnes
Example: 14 / 3 → NTSNEC1200_143

Any

BootP

BootP

Requests IP parameters using the device MAC address from a BootP server.

Any

Stored

Stored IP

Uses saved or default IP address.

Default: 10.10.MAC5.MAC6 (last 2 MAC bytes)

Configurable via Web Server, Control Expert, Machine Expert, or FDR.

Note: Convert MAC from hex to decimal

Any

Clear

Clear / Reset

Clears IP and stored configuration.

Cybersecurity settings remain unchanged.

Requires power cycle and new mode selection to restore communication

rotary selector position

live equipment live equipment

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)

Schneider Electric Nigeria
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings