How can we help you today?

What are the basic machine requirements for installing the EcoSet Design

System Requirements & Compatibility Guide

To ensure optimal performance and a seamless experience, please review the following system requirements before using the application.

Hardware Requirements

Your system should meet or exceed the following minimum specifications:

Memory (RAM): 8 GB or higher

System Type: 64-bit operating system

Storage: Minimum 500 MB of free disk space

Graphics: Basic graphics card

Recommendation: A modern graphics card with hardware acceleration is advised for enhanced performance and visual quality

Display Resolution: Minimum 1280 × 720 pixels

Supported Operating Systems

This application is compatible with the following Windows versions:

Windows 8

Windows 8.1

Windows 10

Windows 11

Note: We recommend using Windows 10 or later for the best performance and security.

Network Requirements

A reliable internet connection is essential for accessing and using the application effectively.

Network Configuration:

IPv4: Required

IPv6: Optional

Required Open Ports:

To ensure uninterrupted connectivity, please allow access through the following ports:

Port 80 (HTTP)

Port 443 (HTTPS)

Schneider Electric Nigeria
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings