How can we help you today?

How do I monitor and diagnose the state of the Unity Momentum CPU communications ?

Issue:

Unity Momentum communication diagnostic LED


Product Line:

Unity Momentum


Resolution:

The LED panel on the 171 CBU 78090 (M1), page 12 processor includes the
following LEDs you can use to diagnose the state of communication over the 2
serial ports:
• MB1 CH0 (yellow)
• MB2 CH1 (yellow)

The LED panel on the 171 CBU 98090 (M1E) and 171 CBU 98091 (M1E-GD)
processors, page 15 includes the following LEDs you can use to diagnose the
state of communication over the serial and Ethernet ports:
• MB1 CH0 (yellow)
• ETH STS (green)
• ETH LNK/ACT (green)
• ETH 100 (green)

The state of each of these LEDs describes the communication status for each
processor, as follows:

image1

Schneider Electric Nigeria

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings