How can we help you today?

How to fix Maximum Connection Reached Error on NMC When Trying To Enter the Web Interface

Issue:

How to fix Maximum Connection Reached Error on NMC When Trying To Enter the Web Interface

This image shows Maximum Connection Reach Error on NMC When trying to Enter Web Interface

Product Line:

Network Management Card 2 (NMC2) - AP9630/AP9631 version 6.x.x above

Network Management Card 3 (NMC3) - AP9640/AP9641 version 1.x.x.x above

Environment:

All serial numbers

Cause:

The "Maximum Connections Reached" error occurs when the Network Management Card (NMC) already has 8 active Web Interface sessions (HTTP/HTTPS). When this limit is reached, no new users can connect until an existing session is closed or times out.

Resolution:

You can clear active or stuck user sessions directly from the NMC CLI. The following steps highlight how to delete active or stuck user session in Web Interface to accept new connections.


1. Open an SSH or Telnet client (e.g., PuTTY) and connect to the NMC IP address.

2. Log in using the NMC username and password.

3. Type "session" to view active connections.

This image shows active sessions in SSH

4. Type "session -d [ID]" to delete a specific session (e.g., session -d 9).
Note: Repeat steps until all unnecessary web sessions have been removed.

This image shows deleting of web active sessions

5. Once no active sessions, exit the CLI or SSH.

6. Re-log in to the NMC Web Interface and confirm that access is restored.

Kindly make sure that "Allow Concurrent Logins" is enabled. You can enable it using web access under Configuration → Security → Session Management. Enable "Allow Concurrent Logins" and click Apply. Verify the setting is saved successfully.

This image shows Session Management allowing Concurrent Log in over the network management card

Note: Allow Concurrent Logins enables multiple users or sessions to be logged in to the NMC simultaneously. When this setting is disabled, only one active login session is permitted at a time, and any additional login attempts may be denied until the existing session is terminated.

Normally, this issue can be resolved by reseating the card or rebooting it through SSH, Telnet or the pinhole button.

Should there be any other questions and/or concerns, feel free to reach out to us at 1-800-800-4272 or our chat with our technical support group atAPC by Schneider Electric Customer Technical Support

Schneider Electric Nigeria
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings