How can we help you today?

How to configure the NMC Data Log Interval and Data Log Size?

Issue:
How to configure the NMC Data Log Interval and Data Log Size?

Product Line:

  • Network Management Card 2 (NMC2) - AP9630/AP9630CH, AP9631/AP9631CH, AP9635/35CH
    pre-2022 2G Metered/Switched Rack PDUs (AP86XX, AP88XX, AP89XX), Rack Automatic Transfer Switches (AP44XX), Certain Audio/Video Network Management Enabled products.
  • Network Management Card 3 (NMC3) - AP9640, AP9641, AP9544
    Devices with an embedded Network Management Card 3 include (but are not limited to): Metered/Switched Rack PDUs (AP84XX, AP86XX, AP88XX, AP89XX, APDU9, APDU10, APDU11, APDU12), Rack Automatic Transfer Switches (AP44XXA), Smart-UPS Online (SRT).

Environment:

  • All serial numbers
  • All firmware versions (unless otherwise specified)

Resolution:
At the default setting, NMC Data Logs has an interval of an averaging of 10 mins. This can cause some measurements to be missed. There will be times when lowering the Data Log Interval to the minimum of 1 minute and setting the Data Log Size to the maximum are helpful in determining or analyzing power issues and gathering closer readings.

To configure the Data Log Interval:

Go to the tab Logs > Data > Interval

Data Log Interval

NOTE: After the data log reaches the maximum size, the oldest entries will be truncated from the log as newer entries are logged.

To configure the Data Log Size:

Go to the tab Logs > Data > Size

Data Log Size

Note: Resizing the Data Log will also delete all current log entries. You may want to offload the Data Log via FTP or SCP before continuing.

For further clarification, please get in touch with the Customer Care Center by clicking on the Green icon Get Help Icon (Get Help) at the bottom right of the website.

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre