How can we help you today?

What calculations does EcoSet Design perform?

1. Short-Circuit Currents

Short-circuit current is the high fault current that flows when a low-impedance path occurs (e.g., 3phase,2phase,1phase faults or phase-to-ground fault).

It is critical for:

Selecting circuit breaker breaking capacity

Ensuring equipment can withstand thermal and mechanical stress

Designing effective protection systems

Accurate calculation prevents equipment damage and ensures safe fault clearing.

2. Voltage Drop Across Circuits

Voltage drop is the reduction in voltage along a conductor due to resistance and impedance.

It increases with:

Cable length

Current magnitude

Conductor resistance

It must be limited to ensure:

Proper equipment operation

Energy efficiency

Compliance with standards

Excessive voltage drop reduces performance and system reliability.

3. Load Currents and Demand

Load current is the current drawn by connected loads, while demand is the maximum expected load at a given time.

Key factors:

Type of load (resistive/inductive)

Diversity factor

Peak vs average load

This helps in:

Proper sizing of transformers and cables

Avoiding overload

Efficient system design

4. Conductor Cross-Sectional Area

Conductor size (mm²) defines its current-carrying capacity.

Selection depends on:

  • Load current
  • Voltage drop limits
  • Installation conditions
  • Thermal capacity

Correct sizing ensures:

  • Safe operation
  • Reduced losses
  • Compliance with standards

5. Protective Device Coordination & Selectivity

Coordination ensures protective devices operate in the correct sequence during faults.

Selectivity ensures:

  • Complementary technical guide.

Methods:

  • Time-based (delay settings)
  • Current-based (trip curves)

Proper coordination improves reliability and prevents total shutdown.

Schneider Electric Nigeria
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings