How can we help you today?

Why BMENUA0100 Syslog Service is not starting using BMENUA0100 version 3.01 and CAE

BMENUA0100 does not support (yet) secured Syslog.


CAE allows us to activate the "Enable security" (and this option is activated by default !!)

CAE

When the NUA receives a cyber  security configuration from CAE with “secured syslog" enabled, the service is not started on BMENUA0100.

CAE

Therefore, before sending a Cyber Security configuration with CAE, please verify that this feature “enabled security” is disabled.

CAE

The Secure Syslog feature will not be available in firmware version 3.01. Its development is scheduled for the next release of the BMENUA0100 firmware.

Product Line

BMENUA0100 version 3.01

EcoStruxure Control Expert 16.4

Cybersecurity Admin Expert version 4.2.1

Schneider Electric Nigeria

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: