How can we help you today?

How to configure automatic variable timestamping on the BMENOP0300 module acting as a server

There are generally three ways to integrate the timestamp corresponding to a Data Object (DO) state change:

  1. Automatic Timestamping

    • The module automatically updates the timestamp value (Data Attribute "t") within the variable.
    • This is only possible when the "t" attribute is not included in the module I/O Mapping.
  2. Manual Timestamping

    • The user manually writes the timestamp value into the Data Attribute "t" through the PLC application and the Device DDT.
    • In this case, the "t" attribute must be included in the module I/O Mapping.
  3. ERT Timestamp Module with SOE Functionality

    • Timestamping can be managed through an ERT timestamp module using the Sequence of Events (SOE) feature.
    • Refer to the product documentation for detailed implementation guidelines.

To enableautomatic timestamping, the Data Attribute "t" must not be mapped in the module I/O Mapping when operating in Server mode. This allows the module to manage and update the timestamp automatically whenever the Data Object changes state.

Consider the Data Object "AlmTOut":

  1. In the I/O Mapping, map only the "stVal" attribute.
  2. Do not map the "t" attribute in the I/O Mapping.
IEDCT screenshot1
3. In the corresponding report dataset, add the "AlmTOut" Data Object and select both the "stVal" and "t" attributes. Including the t attribute in the dataset is required so that the timestamp is published when a report is generated.
4. After inserting the Data Object with both attributes selected, the Attribute column may appear blank. This is normal and expected behavior:

IEDCT Screenshot 3

With this configuration, the module will automatically update the timestamp associated with "AlmTOut" each time its state changes.
IEDScout

Schneider Electric Nigeria

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings