How can we help you today?

What is the cable length from the outside of the battery pack to the connector of BR24BPG?

Question:

What is the cable length from the outside of the battery pack to the connector of BR24BPG?

Product Line:

APC BR24BPG External battery pack

Environment:

All serial numbers

Cause:

The customer is asking for the length of the cable on the battery pack BR24BPG.

Answer:

The cable length from the outside of the battery pack to the connector is :approximately" 30cm / 12 inches.

Image showing the length of the charging cable of a BR24BPG

If you have any clarifications, please feel free to contact us at 1-800-800-4272 or chat with our technical support representatives.

Schneider Electric Nigeria

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings