How can we help you today?

What is the difference between Harmony XB4 and XB5 range ?

1. What you need to know

Both are Ø22 mm Harmony control and signaling units with the same functions, the same mounting cut-out and the same contact blocks. The difference is the head bezel material: XB4 uses chromium-plated metal, XB5 uses plastic. In the reference structure, "4" means metal and "5" means plastic, while "XB" means a complete unit and "ZB" a component. Heads and fixing collars are not interchangeable between the two ranges.

2. How the two ranges are related

XB4 and XB5 are two material variants of the same modular platform. An operator is built from and only the head and fixing collar are range specific.

  • Reference logic: XB4 = complete metal unit, ZB4 = metal component; XB5 = complete plastic unit, ZB5 = plastic component.
  • Contact blocks, light modules and most accessories are common to both ranges.
  • Metal heads mount on metal collars only (ZB4BZ009); plastic heads on plastic collars only (ZB5AZ009).
  • Depending on head type , both ranges can reach up to  IP66, IP67, IP69 and IP69K.
  • Both XB4 and XB5 are rated for harsh environments.

3. Harmony XB4 metal vs Harmony XB5 plastic

Criterion

Harmony XB4 (metal)

Harmony XB5 (plastic)

Bezel and head material

Chromium-plated metal

Plastic

Complete unit prefix

XB4

XB5

Component prefix

ZB4

ZB5

Fixing collar

ZB4BZ009

ZB5AZ009

Body with fixing collar (1 NO)

ZB4BZ101

ZB5AZ101

Degree of protection

IP66, IP67, IP69, IP69K

IP66, IP67, IP69, IP69K

Panel cut-out

Ø22 mm

Ø22 mm

Typical selection driver

Shocks and vibrations resistance, aesthetic

Weight, cost, non-conductive bezel, chemicals

Note : heads and collars cannot be mixed between the two ranges: a ZB4 head does not mount on a ZB5AZ009 collar, and vice versa.

4. Related references

Function

Reference

Description

Complete unit, metal

XB4BA31

Metal pushbutton Ø22, flush, green, 1 NO, screw clamp

Complete unit, plastic

XB5AA31

Plastic pushbutton Ø22, flush, green, 1 NO, screw clamp

Head, metal

ZB4BA3

Metal flush pushbutton head, Ø22, green, spring return

Head, plastic

ZB5AA3

Plastic flush pushbutton head, Ø22, green, spring return

Fixing collar, metal

ZB4BZ009

Metal fixing collar for XB4 / ZB4 heads

Fixing collar, plastic

ZB5AZ009

Plastic fixing collar for XB4 / ZB4 heads

Single NO contact block screw clamp or compact push-in terminals

ZBE101 or 1015

Single NO contact block screw clamp or compact push-in terminals

Single NC contact block screw clamp or compact push-in terminals

ZBE102 or 1025

Single NC contact block screw clamp or compact push-in terminals

Launch Product Selector on se.com to configure a Harmony XB4 or XB5 unit according to your requirements or contact Schneider Electric Technical Support to confirm compatibility with an existing panel.