How can we help you today?

What are the requirements to use the BMENOC0302 with an M580 Safety CPU?

Issue

System requirements


Product Line

M580 Safety


Environment

Control Expert


Resolution

To use the BMENOC0302 with your M580 Safety controller you will need firmware v4.60 on the CPU and must be running Control Expert v16.4.

Schneider Electric Nigeria

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: