How can we help you today?

What report export options are available in EcoSet Design?

EcoSet Design provides the ability to generate comprehensive project reports in PDF format, allowing users to customize the report content according to project and customer documentation requirements. Before exporting, users can choose which sections to include or exclude in the final report.

Available Report Sections

Users can generate reports containing one or more of the following sections:

  • Cover Page
  • Single Line Diagram (SLD)
  • Calculation Notes
  • Bill of Materials (BOM)
  • Cable Schedule
  • Protection System
  • Selectivity Summary
  • Glossary

report

Language Selection

  • Users can select the desired report language prior to report generation.
  • The chosen language is applied consistently throughout the report content and documentation.
  • This feature supports multilingual project documentation for global teams and customers.

Key Benefits

  • Generates project-specific documentation tailored to customer and project requirements.
  • Provides flexibility to include only relevant report sections.
  • Supports multilingual reporting for international projects and stakeholders.
  • Simplifies project review, approval, and documentation processes through standardized PDF reports.

Note: The report export feature enables users to create professional and customized project documentation directly from EcoSet Design, ensuring clear communication of design calculations, protection studies, and equipment details.