How can we help you today?

Understanding microSD Card Requirements on SCADAPack Edge Devices

Summary

SCADAPack Edge devices can operate with Edge firmware without requiring a microSD card. However, a microSD card is required for deploying, storing, and running Edge applications, including Python, C++, Docker-based, and other custom-developed applications.


microSD Cards No Longer Included

microSD cards are no longer supplied with SCADAPack Edge devices. While the hardware continues to include a dedicated microSD card slot, users must provide their own compatible microSD card when application hosting or execution is required.


Is a microSD Card Required for Edge Firmware Installation?

No. A microSD card is not required to install or operate the Edge firmware.

The following functions are available without a microSD card:

  • Installing or upgrading Edge firmware
  • Basic Edge Platform operation
  • Configuring and using Ethernet Ports 3 and 4
  • Using Edge USB interfaces
  • Accessing standard Edge Platform services

As a result, Edge firmware can be installed and run successfully even when no microSD card is present.


When Is a microSD Card Required?

A microSD card becomes necessary when deploying or executing Edge applications. This includes:

  • Python applications
  • C++ applications
  • Docker container applications
  • Custom Edge applications
  • SDK-generated application bundles

Why Is the microSD Card Required?

The Edge Platform uses the microSD card to host critical application-related components, including:

  • Edge Application Overlay: Stores the deployed application bundle and launch scripts.
  • User Read/Write Data: Provides persistent storage for application data.
  • Docker Cache Data: Stores operational and runtime data for containerized applications.

These components make up the Edge Platform's read-write overlay file system and are essential for application execution.

image1

Schneider Electric Nigeria