How can we help you today?

Compact DAP220/250/250C to X80 DDM16022(H) quick wiring - 990XSM00207

Issue

Migrating an ASBDAP220/250/250C to a BMXDDM16022(H) and need to confirm the 990XSM00207 quick wiring cable pinout.

Product line

Modicon X80, M340, M580

Resolution

Below is an image of the pinout.

pinout

Schneider Electric Nigeria

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: